Singapore - Flag Singapore

Please confirm your currency selection:

Singapore Dollars
Incoterms:DDP
All prices include duty and customs fees on select shipping methods.
Free shipping on most orders over $60 (SGD).

US Dollars
Incoterms:DDP
All prices include duty and customs fees on select shipping methods.
Free shipping on most orders over $50 (USD).

Bench Talk for Design Engineers

Bench Talk

rss

Bench Talk for Design Engineers | The Official Blog of Mouser Electronics


Troubleshooting Load-Step Resets in SPE Edge Nodes Stewart Connector / Cinch Connectivity Solutions

(Source: Eakrin/stock.adobe.com)

Electrical devices were once much simpler, operating independently without the need to communicate with the systems around them. A sensor, a light, or an actuator was able to do its job as long as it had a reliable power connection. Most systems were either standalone or part of a simple control loop. Modern systems—especially in buildings and industrial environments—are expected to do much more. They must send data, respond to commands, and sync with just about everything around them. Devices such as lighting systems and environmental sensors are often tied to Ethernet networks so they can be monitored and controlled from a central system. For example, in today’s building systems, lighting must do more than just switch on and off. It is dimmed, scheduled, monitored for energy use, and adjusted in response to data, requiring constant communication between devices.

Conventional Ethernet infrastructure typically uses four twisted pairs and relatively large connectors. While that approach works well in many installations, it can be unnecessarily bulky for deployments with hundreds of sensors, actuators, and lighting nodes, where size, weight, routing space, and installation cost matter.

Single Pair Ethernet (SPE) addresses this problem by using a single twisted pair for Ethernet communication. The cable and connectors are much smaller than conventional Ethernet infrastructure, which makes it easier to connect sensors and other edge devices directly to the network. Power over Data Line (PoDL) delivers electrical power over the same pair used for data transmission. For low-power devices like environmental sensors or light-emitting diode (LED) modules, a single cable can provide both power and data.

Combining power and communication on the same conductors changes how the system behaves during load transitions. Systems that operate normally under steady conditions may respond differently when loads change or when large groups of devices switch simultaneously. The changed response in load transitions can trigger unexpected device resets.

As modern building and industrial systems rely increasingly on SPE and PoDL to deliver both power and communication over a single twisted pair, these load-step resets have become a critical reliability concern. This blog examines why such resets occur by exploring the underlying power‑path and electromagnetic interference (EMI) mechanisms, the diagnostic data needed to pinpoint root causes, and the essential role of cabling and connectors in maintaining stable operation. Additionally, this blog outlines the diagnostic steps and system‑level considerations needed to understand, trace, and mitigate load‑step reset issues in SPE edge-node installations.

A Reset That Appears Only During Load Changes

Consider a building automation system that uses SPE connections to link distributed control nodes. The devices manage lighting zones, collect environmental data, and interact with heating, ventilation, and air conditioning (HVAC) systems. Each node receives power and data through PoDL.

Under normal conditions, the installation appears stable. Devices remain connected to the network and respond correctly to control commands while voltage stays within operating limits.

An issue appears only during scheduled transitions. When lighting scenes change or HVAC equipment begins operating, several nodes reset. The same behavior repeats during each transition. Once the system returns to steady operation, the devices run normally again. The disturbance may last only a few milliseconds and is easy to miss during routine monitoring.

What a Reset Actually Indicates

A reset observed at the device level does not necessarily originate in the microcontroller. Several mechanisms within the system can trigger a restart.

A common cause is a temporary drop in supply voltage. If the input voltage falls below the operating threshold of the processor or Ethernet physical layer (PHY), a brownout reset can occur. Many DC/DC converters also include undervoltage lockout protection that disables the converter when the power supply drops too far.

Startup behavior can produce similar effects, particularly when bulk capacitance must charge as current demand rises. If the power sourcing equipment reaches its current limit during that process, the resulting voltage dip may interrupt the device.

Communication faults can also lead to a restart. EMI or signal integrity problems may cause bursts of packet errors or brief link interruptions. Furthermore, in systems that rely on watchdog timers, prolonged communication loss can trigger a reset.

Identifying the cause of the reset requires information captured during the event itself.

Collecting Useful Diagnostic Data

Troubleshooting usually starts by collecting evidence from both the device and the network. Many microcontrollers record the reason for the last reset. Firmware logs may indicate whether the restart was triggered by a brownout detector, a watchdog timer, or another system condition. This information can help narrow the investigation.

Electrical measurements provide additional clues. Observing the powered device with an oscilloscope can reveal short voltage dips that are easy to miss during normal monitoring. Monitoring the DC/DC converter output and measuring current with a probe or shunt also shows how the device behaves during startup or load changes.

Network infrastructure may also provide useful information. Managed switches often record link events and report packet errors or cyclic redundancy check (CRC) counts, revealing whether communication disturbances occur at the same moment as the reset.

Patterns across the installation are often revealing. Engineers sometimes create a simple table showing the affected nodes, cable lengths, routing paths, and nearby electrical equipment. When resets consistently occur on specific cable runs or in certain areas, the underlying cause becomes easier to identify.

The Source of Reset Events

When diagnostic data is available, the reset behavior often points toward either the power delivery (PD) path or the communication channel. In PoDL-powered SPE systems, voltage disturbances and EMI are two of the most common causes.

When the Problem Lies in the Power Path

If measurements show a voltage drop during the load transition, attention turns to the PoDL power path. Current limiting within the power sourcing equipment may activate when a device begins drawing current. The interaction between PD inrush demand, line impedance, and the power sourcing equipment (PSE) current limit can briefly reduce the available voltage at the powered device.

Cable resistance can also contribute to transient voltage drops. Over longer runs, the resistance of the twisted pair increases the voltage loss when current demand rises quickly. Even if steady-state voltage appears normal, a rapid load change may briefly pull the supply below the device’s operating threshold.

The power path may be affected by the connector and termination quality. Poorly seated connectors or worn contacts add small amounts of resistance, which increases voltage drop during current surges. When several devices switch at the same time, these resistive effects can combine and create brief disturbances that may not appear in slower measurements.

When the Issue Is Electromagnetic Interference

In some installations, the sequence begins with communication errors. Network monitoring may show bursts of CRC errors or brief link interruptions that coincide with the resets. These disturbances often occur when nearby equipment switches on.

Interference can reach the communication path through several routes. Common-mode noise on the cable, grounding inconsistencies, or inadequate shielding may all affect the Ethernet PHY. Cable routing could elevate susceptibility to interference. In fact, SPE cables installed alongside power wiring or switching loads are exposed to stronger electromagnetic fields, increasing the potential for interference.

Identifying the noise source usually requires measurement. Once confirmed, mitigation may involve separating cables, better grounding, or improved shielding continuity.

Connectors in the Signal and Power Path

Connectors are sometimes overlooked during troubleshooting, yet they form part of the electrical and mechanical path between devices.

When the problem involves power delivery, the connector sits directly in the power path. Stable contact resistance helps ensure that transient current events do not introduce additional voltage drops.

If EMI is involved, the connector also contributes to the shield and return path. Reliable shield termination and consistent mating performance help preserve signal integrity across the connection.

Connector systems for SPE installations follow standards such as IEC 63171 and IEC 63171-1, which define the interface dimensions and electrical characteristics required for interoperable connectivity. Stewart Connector / Cinch Connectivity Solutions SPE Connector Systems are designed in compliance with these IEC interface specifications and are used in industrial automation, building infrastructure, and distributed sensing systems.

SPE infrastructure also benefits from the reduced size and weight of single-pair cabling compared with traditional four-pair Ethernet cables. The smaller cable diameter simplifies routing through tight spaces in equipment enclosures, lighting systems, and building infrastructure where large bundles of conventional Ethernet cables would be difficult to manage.

The Stewart Cinch SPE Connector Systems are designed to these specifications, supporting Ethernet variants that include 1000BASE-T1, 100BASE-T1, and the longer-reach 10BASE-T1L and 10BASE-T1S technologies. Compliance with the relevant standards improves the likelihood of cross-vendor interoperability, but actual system compatibility still depends on connector mating, PHY implementation, channel compliance, PD design, and application constraints.

Because SPE uses a single twisted pair, internal pair-to-pair crosstalk within the cable is eliminated. However, engineers must still consider external electromagnetic coupling and alien crosstalk when SPE cables are bundled alongside other communication or power conductors.

Some SPE PHY variants enable longer link distances than traditional Ethernet installations. For example, 10BASE-T1L can reach distances approaching 1000m with the correct cabling. When PoDL is used simultaneously for power delivery, the additional current flowing through the cable can reduce practical distance margins, making power integrity and connector performance even more important.

Conclusion

When resets appear during load transitions, the cause often lies in short disturbances that occur in the power delivery path or in the communication channel. Capturing voltage and current during these events helps indicate where the disturbance starts. Network activity can provide additional clues about what is happening at the same time. With that information, the system path, which includes cabling and connectors, can be examined to determine the source of the reset. Fortunately, connector systems exist that follow interface specification standards that ensure interoperable connectivity and help mitigate device resets caused by load transitions.

Author

David Pike is well known across the interconnect industry for his passion and general geekiness. His online name is Connector Geek.



« Back


The Stewart Connector portfolio of products from Bel include one of the broadest ranges of Ethernet connectivity. The company's interconnect products include passive jacks, plugs and cable assemblies that provide connectivity in networking equipment.


All Authors

Show More Show More
View Blogs by Date

Archives