Mouser Electronics Now Shipping Renesas RX23W BLE Module for IoT System Control

New Product Announcement

Connect With Us


July 26, 2021Mouser Electronics, Inc., the authorized global distributor with the newest semiconductors and electronic components, is now stocking the RX23W module with built-in antenna and oscillator from Renesas Electronics. The compact 6.1 mm × 9.5 mm module offers full Bluetooth® 5.0 Low Energy support for system control and wireless communication on Internet of Things (IoT) endpoint devices.

The Renesas RX23W module, available from Mouser Electronics, incorporates the RX23W microcontroller to support full Bluetooth 5.0 Low Energy communication, including long-range and 2 Mbps data throughput and a reception sensitivity level of −105 dBm at 125 kbps. The module is available with Renesas’ exclusive security function, the Trusted Secure IP, which provides robust protection against threats such as eavesdropping, tampering, and viruses. And with Radio Law (Japan), FCC/ISED (North America), CE (Europe), and Bluetooth SIG certifications, the RX23W module removes the need for additional RF design work, tuning, or specialized RF knowledge, shortening new product development time.

Applications for the RX23W module include healthcare, smart home appliances, building automation, PC and smartphone peripherals, industrial and IoT designs. For development, Mouser also stocks the RX23W Module Target Board, which incorporates the RX23W module, two 36-pin headers for access to all signals, and a USB port for PC connectivity for programming and debugging.

To learn more about the Renesas RX23W module, visit https://www.mouser.com/new/renesas/renesas-rx23w-ble-module/.

 

As a global authorised distributor, Mouser offers the world's widest selection of the newest semiconductors and electronic components — in stock and ready to ship. Mouser's customers can expect 100% certified, genuine products that are fully traceable from each of its manufacturer partners. To help speed up the design process for customers, Mouser's website hosts an extensive library of technical resources, including a Technical Resource Centre, along with product data sheets, supplier-specific reference designs, application notes, technical design information, engineering tools and other helpful information.

About Mouser

2026 - Mouser Electronics is an authorized semiconductor and electronic component distributor focused on New Product Introductions from its leading manufacturer partners. Serving the global electronic design engineer and buyer community, the global distributor's website, mouser.com, is available in multiple languages and currencies and features more than 6.8 million products from over 1,200 manufacturer brands. Mouser offers 28 support locations worldwide to provide best-in-class customer service in local language, currency and time zone. The distributor ships to over 650,000 customers in 223 countries/territories from its 93,000m², state-of-the-art distribution facilities in the Dallas, Texas, metro area. For more information, visit https://www.mouser.com.

Trademarks

Mouser and Mouser Electronics are registered trademarks of Mouser Electronics, Inc. All other products, logos, and company names mentioned herein may be trademarks of their respective owners.

For further information, contact:
Kevin Hess, Mouser Electronics
Senior Vice President of Marketing
+1 (817) 804-3833
For press enquiries, contact:
Kelly DeGarmo, Mouser Electronics
Manager, Corporate Communications and Media Relations
+1 (817) 804-7764