Selecting RF Chip Capacitors for Wireless Applications
By Richard Fiore, Director of RF Applications Engineering, American
Technical Ceramics Corp
With today’s advancements in wireless technology, greater emphasis is being placed on component
performance. This article will provide a discussion of ceramic and porcelain chip capacitors and understanding
their behavior in RF product designs. They are an excellent choice for wireless applications where volumetric
efficiency, reliability and RF performance are an absolute must.
Design Criteria
The most commonly used design categories for ATC ceramic chip capacitors are the multilayer (MLC) and single
layer (SLC). T he MLC employs multiple or stacked electrode sections while the SLC consists of two electrodes
separated by a dielectric. Both are constructed with the following design criteria:
- Ceramic and porcelain dielectrics
- Rugged hermetic construction
- Optimized electrode patterns
- Low resistivity electrode and termination materials
- High dielectric strength
- Protective barrier layer between electrodes and termination (MLC)
- Fabricated for direct surface mounting on microstrip
- Ultra stable with temperature and humidity
- Extremely high Q
- Low dissipative losses
Selecting a Suitable Capacitor
When selecting ceramic chip capacitors for use in RF wireless applications, it is important to establish overall
circuit performance criteria. The component should then be matched to the specific application requirement. A
typical shopping list of performance requirements for this circuit element may include the following:
- Capacitance (pF)
- Tolerance (%)
- Voltage Rating (WVDC, VRMS)
- Equivalent Series Resistance (ESR)
- Temperature Coefficient (TC, PPM/°C)
- Dissipation Factor (%)
- Series Resonant Frequency (Fsr)
- Parallel Resonant Frequency (Fpr)
- Insulation Resistance (IR)
- Dielectric Aging Effects (% per decade hr.)
Performance
An ideal capacitor stores all of its energy in the dielectric, as 1/2CV². However, a realizable capacitor
will always exhibit some series resistance that must be taken into account. This series resistance referred to
as Equivalent Series Resistance (ESR) is always one of the most essential factors to consider in an RF circuit
design. It is attributed mainly to the contribution of dielectric losses, and metal losses of electrode and
termination materials. Also, the manufacturing process must be properly controlled during every phase to insure
optimal ESR performance. At low frequencies, Hz to KHz region, the main contributor to ESR is dielectric loss.
However, at RF frequencies the ESR is due mainly to the metal losses, i.e., electrodes and terminations. These
losses become significant because of skin effect and increase proportionally as the square root of frequency.
ESR is typically expressed in milliohms at specific frequencies by most manufacturers. The standards most
frequently used as a guideline are EIA RS483 and MIL-C-55681. The measurements are performed at various
frequencies between 30 MHz and 1 GHz. Therefore, it is necessary to consider the ESR value at your specific
design frequency. If, for example, you are designing for a 900 MHz wireless application, and the ESR is
specified at 150 MHz, the ESR at 900 MHz may be calculated by multiplying the specified ESR at 150 MHz by
√ 900/150 . This relationship is well behaved at
RF and accounts for the "skin effect". The ESR is the main loss element of the capacitor and is used
to determine the power loss i.e.; P = I²*ESR.
Quality Factor (Q) is a figure of merit and is a measure of a capacitor's ability to store energy in its
dielectric. Since Q = Xc / ESR, it becomes evident that low ESR yields high Q. As with ESR, the Q must be
specified or calculated at the design frequency.
Dissipation Factor (DF) is also referred to as the loss tangent and is the reciprocal of Q, i.e., DF = 1/Q. With
an ideal capacitor the current leads the voltage by 90 degrees. However, actual capacitors will have a small
angle referred to as the loss angle. The tangent of the loss angle is equal to the dissipation factor and
indicates what portion of the total reactive power in the capacitor will be lost as heat i.e., dissipative loss.

Figure 1. Dissipation Factor
Example: loss angle = 3 degrees;
therefore DF = tan 3 = 0.05 or 5%.
In the above example, the dissipation factor is 0.05 or 5%. This means that 5% of the total power in the
capacitor is lost as heat. Refer to Fig. 1.
The ATC 100 Series porcelain chip capacitors have a loss tangent less than 0.0001 that yields a Q greater than
10,000. In this instance the dissipative losses are less than 0.01%. This is desirable for optimum performance
in an RF circuit. An amplifier circuit for example, that utilizes a high Q, low ESR (DF) capacitor will realize
a significant increase in the effective gain. Battery life for portable devices is also extended with the use of
low loss capacitors. An easy way to relate ESR, DF and Q together is:
ESR = Xc DF = Xc /Q
DF = ESR /Xc
Q = Xc /ESR
Parasitic Behavior
Another major concern in wireless design applications is the parasitic behavior of the reactive elements.
Capacitors may be modeled with equivalent circuit elements that account for the parasitic effects. Figure 2
shows a lumped element model and is valid for chip capacitors in these applications. Using this model can help
the designer determine such characteristics as the series resonant frequency (Fsr), equivalent series inductance
(ESL) and transfer function characteristics.

Figure 2. Equivalent Circuit Model
It is necessary to consider the functional application, e.g., coupling, bypass, timing etc., and layout in the
circuit. For example, a given application may require a capacitor for interstage coupling. A more thorough view
of parasitic behavior is accomplished by the use of scattering parameters. ATC specifies S-Parameter performance
for their capacitor line. This data may be downloaded from ATC’s website and is also available on
ATC’s CD Catalog.
In the above example it is important to evaluate the S-Parameter performance for the subject capacitor. If a
parallel resonance occurs at or near the frequency band of interest, this capacitor will serve to attenuate the
RF energy rather than it’s intended coupling function. S-Parameter data will show such characteristics as
parallel resonance, series resonance, insertion loss, insertion phase, return loss magnitude and return loss
phase. A full set of SParameters may be used in conjunction with design simulation software, and is generally
presented as a forward and reverse two port measurement known as an S2P file.
Component Orientation
Chip capacitors are usually surface mounted on a microstrip. They can be mounted with the electrodes parallel or
perpendicular to this microstrip. In the above example a coupling capacitor is used between stages. As
previously mentioned it is essential that parallel resonances do not occur in the frequency band of interest. By
mounting the capacitor vertically, that is, with the electrodes perpendicular to the microstrip, the first
parallel resonance will not be present thereby significantly extending the usable bandpass. A comparison of the
two mounting orientations using S-Parameters is shown in Figure 3.

Figure 3. S-Parameter Plots comparing horizontal and verticalmounting orientations
Series Resonant Frequency: Occurs at the frequency corresponding to 0 degrees phase of S21; also S21 magnitude
has minimum loss at this frequency equal to ESR.
Parallel Resonant Frequencies: Are observed as a sharp attenuation in the S21 magnitude while S21 phase has rapid
transitions through 0 degrees corresponding to each parallel resonance. Vertical mount ing optimizes this
performance.
S21 Magnitude 3DB Frequency: Capacitance value may be verified at this frequency by C = 0.159/100*F (Hz).
Author Bio
Richard Fiore has 38 years of experience
in RF engineering. His professional experience includes a wide range of areas such as design and implementation
of RF automated test systems for the defense electronics industry, filter design for both military and
commercial markets, CATV System design, EMC/RFI design and testing, design, prototype and evaluation of RF
components, modules and systems. He is presently Director of RF Applications Engineering at American Technical
Ceramics in Huntington Station, NY and has been with the company since April 1994.
Reprinted with permission from Wireless Design & Development